Thanks Petr
I understand that FlexCAN and MSCAN are low level drivers that help set the bit rate, buffer sizes and callback functionality etc.? And the FreescaleCAN is the high level driver that will save us time in constructing/deconstructing and parsing the data into/from our required proprietary CAN protocol messages?
I am needing the message format to be configurable, using AmsCAN, a high level proprietary CAN protocol, based on 1 Mbit/sec, 11-bit identifiers, fairly simple, standard message types: READ, WRITE, COMMAND, receive STATUS update.
i.e. NOT locked into a high level "CANopen" protocol. Are you able to confirm that these drivers are configurable and flexible enough to do this? I have spent ages dredging through the website and can't find much more detail.
We currently use CodeWarrior 4.2.6 with SDK 2.5. Is it too hopeful to expect that the high level driver is still available for this version? We have heaps of code based around this, (though sounds like the beans are MUCH easier to use than SDK).
I presume that Processor Expert, basic and advanced beans will not work with our older version of CodeWarrior, so we would need a 30 day trial version of CodeWarrior Basic or Standard + the advanced bean for FreescaleCAN?
Thanks again
Michael Tibbs
Learner!