#include "lpc17xx.h"
#include "type.h"
#include "uart.h"
volatile uint32_t UART0Status, UART1Status;
volatile uint8_t UART0TxEmpty = 1, UART1TxEmpty = 1;
volatile uint8_t UART0Buffer[BUFSIZE], UART1Buffer[BUFSIZE];
volatile uint32_t UART0Count = 0, UART1Count = 0;
void UART0_IRQHandler (void)
{
uint8_t IIRValue, LSRValue;
uint8_t Dummy = Dummy;
IIRValue = LPC_UART0->IIR;
IIRValue >>= 1; /* skip pending bit in IIR */
IIRValue &= 0x07; /* check bit 1~3, interrupt identification */
if ( IIRValue == IIR_RLS ) /* Receive Line Status */
{
LSRValue = LPC_UART0->LSR;
/* Receive Line Status */
if ( LSRValue & (LSR_OE|LSR_PE|LSR_FE|LSR_RXFE|LSR_BI) )
{
UART0Status = LSRValue;
Dummy = LPC_UART0->RBR;
return;
}
if ( LSRValue & LSR_RDR ) /* Receive Data Ready */
{
UART0Buffer[UART0Count] = LPC_UART0->RBR;
UART0Count++;
if ( UART0Count == BUFSIZE )
{
UART0Count = 0; /* buffer overflow */
}
}
}
else if ( IIRValue == IIR_RDA ) /* Receive Data Available */
{
UART0Buffer[UART0Count] = LPC_UART0->RBR;
UART0Count++;
if ( UART0Count == BUFSIZE )
{
UART0Count = 0; /* buffer overflow */
}
}
else if ( IIRValue == IIR_CTI ) /* Character timeout indicator */
{
/* Character Time-out indicator */
UART0Status |= 0x100; /* Bit 9 as the CTI error */
}
else if ( IIRValue == IIR_THRE ) /* THRE, transmit holding register empty */
{
/* THRE interrupt */
LSRValue = LPC_UART0->LSR; /* Check status in the LSR to see if
valid data in U0THR or not */
if ( LSRValue & LSR_THRE )
{
UART0TxEmpty = 1;
}
else
{
UART0TxEmpty = 0;
}
}
}
void UART1_IRQHandler (void)
{
uint8_t IIRValue, LSRValue;
uint8_t Dummy = Dummy;
IIRValue = LPC_UART1->IIR;
IIRValue >>= 1; /* skip pending bit in IIR */
IIRValue &= 0x07; /* check bit 1~3, interrupt identification */
if ( IIRValue == IIR_RLS ) /* Receive Line Status */
{
LSRValue = LPC_UART1->LSR;
/* Receive Line Status */
if ( LSRValue & (LSR_OE|LSR_PE|LSR_FE|LSR_RXFE|LSR_BI) )
{
/* There are errors or break interrupt */
/* Read LSR will clear the interrupt */
UART1Status = LSRValue;
Dummy = LPC_UART1->RBR; /* Dummy read on RX to clear
interrupt, then bail out */
return;
}
if ( LSRValue & LSR_RDR ) /* Receive Data Ready */
{
/* If no error on RLS, normal ready, save into the data buffer. */
/* Note: read RBR will clear the interrupt */
UART1Buffer[UART1Count] = LPC_UART1->RBR;
UART1Count++;
if ( UART1Count == BUFSIZE )
{
UART1Count = 0; /* buffer overflow */
}
}
}
else if ( IIRValue == IIR_RDA ) /* Receive Data Available */
{
/* Receive Data Available */
UART1Buffer[UART1Count] = LPC_UART1->RBR;
UART1Count++;
if ( UART1Count == BUFSIZE )
{
UART1Count = 0; /* buffer overflow */
}
}
else if ( IIRValue == IIR_CTI ) /* Character timeout indicator */
{
/* Character Time-out indicator */
UART1Status |= 0x100; /* Bit 9 as the CTI error */
}
else if ( IIRValue == IIR_THRE ) /* THRE, transmit holding register empty */
{
/* THRE interrupt */
LSRValue = LPC_UART1->LSR; /* Check status in the LSR to see if
valid data in U0THR or not */
if ( LSRValue & LSR_THRE )
{
UART1TxEmpty = 1;
}
else
{
UART1TxEmpty = 0;
}
}
}
uint32_t UARTInit( uint32_t PortNum, uint32_t baudrate )
{
uint32_t Fdiv;
uint32_t pclkdiv, pclk;
if ( PortNum == 0 )
{
LPC_PINCON->PINSEL0 &= ~0x000000F0;
LPC_PINCON->PINSEL0 |= 0x00000050; /* RxD0 is P0.3 and TxD0 is P0.2 */
/* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
/* Bit 6~7 is for UART0 */
pclkdiv = (LPC_SC->PCLKSEL0 >> 6) & 0x03;
switch ( pclkdiv )
{
case 0x00:
default:
pclk = SystemFrequency/4;
break;
case 0x01:
pclk = SystemFrequency;
break;
case 0x02:
pclk = SystemFrequency/2;
break;
case 0x03:
pclk = SystemFrequency/8;
break;
}
LPC_UART0->LCR = 0x83; /* 8 bits, no Parity, 1 Stop bit */
Fdiv = ( pclk / 16 ) / baudrate ; /*baud rate */
LPC_UART0->DLM = Fdiv / 256;
LPC_UART0->DLL = Fdiv % 256;
LPC_UART0->LCR = 0x03; /* DLAB = 0 */
LPC_UART0->FCR = 0x07; /* Enable and reset TX and RX FIFO. */
NVIC_EnableIRQ(UART0_IRQn);
LPC_UART0->IER = IER_RBR | IER_THRE | IER_RLS; /* Enable UART0 interrupt */
return (TRUE);
}
else if ( PortNum == 1 )
{
LPC_PINCON->PINSEL4 &= ~0x0000000F;
LPC_PINCON->PINSEL4 |= 0x0000000A; /* Enable RxD1 P2.1, TxD1 P2.0 */
/* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
/* Bit 8,9 are for UART1 */
pclkdiv = (LPC_SC->PCLKSEL0 >> 8) & 0x03;
switch ( pclkdiv )
{
case 0x00:
default:
pclk = SystemFrequency/4;
break;
case 0x01:
pclk = SystemFrequency;
break;
case 0x02:
pclk = SystemFrequency/2;
break;
case 0x03:
pclk = SystemFrequency/8;
break;
}
LPC_UART1->LCR = 0x83; /* 8 bits, no Parity, 1 Stop bit */
Fdiv = ( pclk / 16 ) / baudrate ; /*baud rate */
LPC_UART1->DLM = Fdiv / 256;
LPC_UART1->DLL = Fdiv % 256;
LPC_UART1->LCR = 0x03; /* DLAB = 0 */
LPC_UART1->FCR = 0x07; /* Enable and reset TX and RX FIFO. */
NVIC_EnableIRQ(UART1_IRQn);
LPC_UART1->IER = IER_RBR | IER_THRE | IER_RLS; /* Enable UART1 interrupt */
return (TRUE);
}
return( FALSE );
}
void UARTSend( uint32_t portNum, uint8_t *BufferPtr, uint32_t Length )
{
if ( portNum == 0 )
{
while ( Length != 0 )
{
/* THRE status, contain valid data */
while ( !(UART0TxEmpty & 0x01) );
LPC_UART0->THR = *BufferPtr;
UART0TxEmpty = 0; /* not empty in the THR until it shifts out */
BufferPtr++;
Length--;
}
}
else
{
while ( Length != 0 )
{
/* THRE status, contain valid data */
while ( !(UART1TxEmpty & 0x01) );
LPC_UART1->THR = *BufferPtr;
UART1TxEmpty = 0; /* not empty in the THR until it shifts out */
BufferPtr++;
Length--;
}
}
return;
}
|