Content originally posted in LPCWare by Ex-Zero on Wed Nov 14 10:23:36 MST 2012
Quote: micronpn
So the problme is that I have no liblinks.xml file in both libraries directories.
Your lib directory doesn't include liblinks.xml :confused::eek::confused:
How did you create it ?
Note: "Smart update" is a function, which can be used to add library settings to a project :) It's faster and easier than doing that manually (= adding path to 'Includes','Libraries' and 'Paths and Symbols'). 'Smart Update' is writing these things to Debug and Release Configuration of every selected project. Therefore 'liblinks.xml' is created in a 'C Static Library Project', which is including this information.