Content originally posted in LPCWare by Harrzack on Tue Aug 05 06:18:49 MST 2014
Greets to all!
I'm coming from the Arduino world and trying to 'translate' how the include files should be structured. In Arduino, a 'library' is a c++ class which you can include in your 'sketch' (program). There is a default path to a folder named 'libraries' where the files for these classes are held. Looking at these files, they look suspiciously just like the files & folders in the LPCOpen1549 folder.
This is also my first foray into the more disciplined world of c++ via the LPCXpresso IDE. It seems each time a workspace is created, all needed library files are COPIED into the new workspace. While storage isn't a big deal, this does seem a bit wasteful.
Can a path be created such that I can point to one copy of the LPCOpen1549 library, and create one of my own for my custom libraries - and have the paths as system defaults for any workspace that is created?
=Alan R.
----------------------------------