Content originally posted in LPCWare by Meyer on Thu Sep 19 06:11:09 MST 2013
Hi noahk,
I am using the Hitex Eval Board Lpc4350 with exactly this Spansion S25FL129P. Memory Region is correct ,register base address is 0x40003000.
In my opinion it should be run. When I run the entire code from the ram, then I can read and write out of flash as I'm funny.
I guess the problem is switching back to spifi for execution. Cause when debugging i saw the new value written in flash but after that i got error
fffffffe: Unable to retrieve disassembly data from backend. No source available
100000004: Unable to retrieve disassembly data from backend.
if you have the same board, I can send my project.
If anyone has an idea; bring it on ;)
Thx