lpcware

53: License does not permit flash operations from the command line?

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by mosesmck on Fri Oct 08 11:30:33 MST 2010
Hi,

I just got an LPCXpresso with the LPC1114 chip on it, and I'm using LPCXpresso for Linux Beta 2 on Ubuntu 10.04.  I compiled the "Blinky" example in debug mode and tried to write it to the chip using the "Program Flash" button, and it gives me the following error in a message box:

"53: License does not permit flash operations from the command line"

I got the license for the free version of LPCXpresso, and the welcome page tells me:

"Welcome to LPCXpresso.  The software is now fully activated, and can be used for production.  LPCXpresso can be used to generate and download applications containing up to 128K of code into an LPC target."

I was able to run the program in Debug mode and that wrote the program to the chip, but I really would like to be able to just program the flash.  Does anyone know what might be the problem?

Thanks,
Moses

Outcomes