Content originally posted in LPCWare by internav on Tue Jan 28 18:58:35 MST 2014
Hi,
My mistake, the flash was corrupt.
Now with the secondary bootloader and my program in flash, I can attach and debug.
But now the uart interrupt routine returns to neverland. If my program is linked with the default script, ir runs fine in standalone mode. With my script, it returns wrong. here are the script files. The code begins at 0x2000 and the bootloader has been changed from the normal 0x1000 to 0x2000 for the redirection.
added later:
I am using the system tick and that interrupt works fine. Neither the systick or uart isrs are used in the bootloader.
tell me what other details you want.