Content originally posted in LPCWare by Luis Digital on Fri Oct 01 19:53:21 MST 2010
Quote: tkreyche
I was expecting a better looking square wave from the CLKOUT pin...see photo for 4 MHz output. No problem running it through a clock buffer to clean it up, but still.
I'm considering using it to drive an external ADC.
Image is from my Tectronix 2445 150 MHz scope.
Comments?
What is the output of another microcontroller that operates at 4 MHz and 3.3 volts?
I have the same plans, but at 50 MHz, and my ADC is 5.0 volts, so I'll need a buffer. Any recommendations about the buffer is welcome.