Content originally posted in LPCWare by pig_man on Mon Sep 20 09:40:18 MST 2010
I tried to boot my board with LPC1767 with the source code (LPCXpresso1768_systick_twinkle) from the LPC1768 reference board (with the processor setting changed to LPC1767) . I kept getting this message:
LPCXpresso Debug Driver v2.0 (Aug 31 2010 23:37:18)
Looked for chip XML file in D:/nxp/lpcxpresso_3.5/bin/LPC1767.xml
Looked for vendor directory XML file in D:/nxp/lpcxpresso_3.5/bin/nxp_directory.xml
Found generic directory XML file in D:/nxp/lpcxpresso_3.5/bin/crt_directory.xml
Emu(0): Conn&Reset. DpID: 2BA01477. Info: T1S6RGRIA
SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Packet delay: 0 Poll delay: 0.
XML Error in directory file D:/nxp/lpcxpresso_3.5/bin/nxp_lpc17xx.xme on line 196: Element enclosed in invalid element nesting: 'peripheralInstance'.
03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part
I verified the Part ID is 0x26012837, so the LPC-link is talking to the device correctly. However, I can't get any further. Do I have to use LPC1768 with LPC-link? Did I miss something else?
Thank you.