lpcware

Interfacing LPC1769 to PL2303 or CP2102 based USB to serial converter

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by suhel on Mon Nov 10 12:21:15 MST 2014
Hi,

I have an issue, very trivial, i am a newbie.

I want to interface LPC1769 to PC. And for that purpose i have bought a PL2303 module and i also have a CP2102 based USB to serial converter.

If i am correct LPC1769 works on 3.3v.

When i measure the voltage on the Tx and Rx lines on the USB to serial converter i see that it i s ~5v.

Can i connect these modules to UART TX and Rx on the LPC??

will the 5v harm the IO pins??

Please answer.

Regards,
Suhel

Outcomes