Content originally posted in LPCWare by gusika on Wed Nov 02 03:18:18 MST 2011
From a serious error. There are two operating systems I tried, one worse than the other. From one moment to another, resulting in failure.
w7/x64-re fresh installation: create new workspaces, create new project, LPCXpressoC, select processor, etc. Open main.c file, click Build command is the first error is: "Building file: .. / src / aeabi_romdiv_patch.s" file not found error
VBox/XP/32-re fresh installation: create new workspaces, create new project, LPCXpressoC, select processor, etc. Open main.c file, click on build: the last command is an error: "Performing post-build steps," file not found error
But before it was set up. AXF file!
Simply doing what is impossible in this program.