Content originally posted in LPCWare by Ronald on Sat Nov 05 05:33:59 MST 2011
Thank you, the project is now compiled without any error or warning, however I can't flash anymore. I could before.
Pc: ( 0) Reading remote configuration
Ni: LPCXpresso Debug Driver v4.0 (Sep 21 2011 20:05:40)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/LPC1765.xml
Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/nxp_directory.xml
Nc: Found generic directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/crt_directory.xml
Pc: ( 5) Remote configuration complete
Ed:02: Failed on connect: Em(01). Cannot find selected MEM-AP (check target power)
Et: Emu(0): Conn&Reset. Was: None. DpID: 2BA01477. Info: T1S6RGRIA
Error 0: (null)
Last sticky: 17. AIndex: 0
No MemAp selected
No Speed test
SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Packet delay: 0 Poll delay: 0.
Pc: (100) Target Connection Failed
This is the response