Content originally posted in LPCWare by andrews on Tue Oct 29 09:03:35 MST 2013
Is there a PCB layout drawing available for the LPCxpresso LPC1769 Rev B board? It doesn't appear all the pins that are supposed to be connected to the expansion connector are connected based on the schematic I have. For example, P0.22 does not go to the expansion connector on my board. I could have a problem with my board but want to make sure the board is really laid out as shown in the schematic.
Thanks