Content originally posted in LPCWare by martinho on Thu Mar 31 02:56:06 MST 2011
Thanks for Your help,
TheFallGuy: Yes I did see the other post's (at least most of them) but non of there solutions seems working for me.
larryvc: My board is powered by a 3.3V regulator (voltage is OK) and i'm debugging with the LPC-Link (without CPU Board attached). The same HW was working in past.
I do not understand why the Debugger tries to write at 0x0300FFFD (where he clearly don't find memory or peripherals). I have tried to program the board with the untouched FreeRTOS example from NXP with the same error. Unfortunately i do not have other Boards at then moment, but i will try it on a other board as soon as possible.
thanks
Martin