Content originally posted in LPCWare by kemayou21 on Mon Jan 05 03:11:22 MST 2015
i want to convert two different Input voltage at the same time but after the conversion is done i become only one of the two value. Can someone please help me know what i going wrong.
Thx
AD_sel_base->ADCR |= 0x01200303;// AN0.0, 14,4MHz/4, PDN ON, START
AD_0 = (AD_sel_base->ADDR0 >> 6) & 0x3FF;
AD_1 = (AD_sel_base->ADDR1 >> 6) & 0x3FF;
AD_sel_base->ADCR |= 0x01200303;