lpcware

appending a revision/build code at end of ROM

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by agemoz on Fri Jan 02 10:53:16 MST 2015
I'm porting a FW design to the NXP LPC4357.  I used to use the GCC toolchain by entering in command prompt text (or running simple scripts), but now am learning how to use LPCXpresso.  Things are going pretty well but one of the things I used to do was append a revision/build code file at the end of the ROM code object.  I searched the FAQ and this forum but don't see how to control the ordering of object files in a link.  I would guess one way is to manually edit the link file.  Is there a better way to control the ordering of linked objects and still be able to use the managed linker script option?

Thanks Robert

Outcomes