lpcware

"timeout waiting for Redlink Server to initialise(1)" on Mac mini running OS 10.9.4

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by ianleslie on Tue Sep 30 07:38:32 MST 2014
I am running LPCXpresso 7.4.0 and using LPC-Link2 powered from a powered hub.

I frequently get the error

"timeout waiting for Redlink Server to initialise(1)"

The only way around this error is to reboot the Mac and then all works fine for a while.  (That, is power cycling the board and exiting and restarting LPCXpresso doesn't solve the problem.)

Is there a way to reset the Redlink drivers, etc without rebooting and/or is there something I should be doing to get more diagnostics?

Thanks



Outcomes