Content originally posted in LPCWare by richard parker on Thu Jun 26 13:32:05 MST 2014 This is a completely stupid and very basic question I know. This is what happens when a hardware guy has to start playing with software :/
I want to download code onto a Keil MCB4357 with examples from LPCXpresso. Do I need to use a ULINK2 or can I use the LPC-LINK2 or even the Segger J-LINK? As you may gather I only have the MCB4357 evaluation board and not the board with the ULINK-ME. How do I see what hardware debug tool is selected? So far I have only used example projects using the inbuilt LPC-LINK2 on other Xpresso boards and this is my first foray into a non xpresso board.
Content originally posted in LPCWare by mc on Thu Jun 26 14:45:50 MST 2014 Hi RIchard, MCB4300 board has Cortex Debug connector(J6). Connect LPC Link2 connector (J7) to MCB4300 connector J6.
Content originally posted in LPCWare by richard parker on Thu Jun 26 14:03:25 MST 2014 So if I plug a JTAG lead from, say, an LPC-LINK2 into the MCB4357 it will work? Is there anywhere that I need to select the probe for the project?