lpcware

Run LPCXplorer 1830 without JTAG

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by ArriaLive on Sat Oct 12 22:51:36 MST 2013
I know there has to be a simple answer to this, but I can't seem to find it.

I have a small program running decently well on the LPCXplorer 1830 board using the LPCXpresso JTAG interface with the LPCXpresso Eclipse IDE to load the program into flash.  It works great.

I would like to have the Xplorer board boot up when powered on to run the program without having to load it each time using the Xpresso debug option.  In other words, I just want to remove the JTAG board, and have the Xplorer just boot up when powered on and execute the code loaded in the last time.

When I just try to power the Xplorer up, there is no indication that the software is functioning (I have the LED's blinking when the program is running).

I know there must be a simple way to power on directly to my code, but I can't figure it out.  Any hints?

Thanks!

Outcomes