Content originally posted in LPCWare by Izzy Weird on Wed Aug 24 13:29:17 MST 2011
Quote: Rob65
My impressions are a bit different.
I have no problem at all opening a [I]workspace[/I].
Note that I don't open project files; instead I just start the LPCXpresso IDE and select my workspace....
That was the obvious thing, I opened the workspace. But no project files showed up in the project window. Perhaps some wizard failed the first time, but as I said I had a working project yesterday. How does one save a project before exiting Code Red?
Quote: Rob65
Sure, and I have numerous tools to prove that this is not the way to go forward ... When I click a.c or .h file it should open in textpad since that is the editor I assigned this filetype to.
But ... All these fancy IDE tools think they are the master of all and they need to open this file. So on one PC I'm stuck with my .c files in Visual C, on another PC it's C++ Builder and then I also have a number of embedded tools that could open the file - all depending on which tool I installed last.
...
I have had this problem when I have multiple versions of one IDE, like IAR installed. But clicking on an IAR project only brings up IAR, not Keil etc. These IDEs are all incompatible enough that usually one one can be used with most projects.
Quote: Rob65
If it hurts when you press with your finger on a part of your body (any part)
then maybe - maybe ... it's your finger that's hurting :eek:
Have you tried different USB cables ???
...
The cable I borrowed was from an ST-Link, and it seems pretty stable, I'll try another. But I'll bet you (either the Code Red driver or) the hardware is not as stable as most JTAG interfaces like SAM-ICE, Segger, or ST-Link, etc.
Quote: Rob65
I have 4 PCs (1 desktop, 1 all in one and 2 laptops) with the LPCXpresso IDE installed. I have used different versions ranging from 3.2 to 4.0.6 on all of these and they all work like a charm (but please read on).
Blame this on Microsoft.
Is it not strange the OS lets us create a directory structure it is unwilling to delete :confused:
I've seen this before with one of my own programs that created funny directory structures. But I was still able to delete the whole tree with the CygWin tools - In my case a real Windows UI problem.
...
I loaded Cygwin to try to solve this. (It purported to give me the power of Linux in Windows.) It accepted my command, but did absolutely nothing. I won't blame Microsoft for that, a lot of open source stuff is free and worth every penny. The final fix (in a post below) was done totally from Windows, so I guess I should thank Microsoft for that.
Quote: Rob65
Don't get me wrong. There are indeed problems with the LPCXpresso IDE.
It works like a charm but as with any spell, they don't always do exactly what you want them to do ...
I still don't get it why we have to specify stuff like include files for both debug and release mode. And having to specify the location of the include file, the location of the library file and the name of the library file for a library module seems a bit superfluous but then, this is exactly as I was used to do so in my own makefiles on other (Unix) make environments :rolleyes:
Still, if you have specific questions/problems, feel free to post again. I'll switch of my turkey alarm and try to answer them in a more serious manner :D
Rob
P.s: I spent most of today trying to get a > 10,000 USD mechanical CAD application to behave properly. Somehow the program does not want to accept my models and the 2,000 USD/year customer support can't provide me with a solution ...
I hear you, another engineer here is fighting with Cadence PCB CAD. Sometimes software gets to a point where it has been hacked and modified so thoroughly that it needs a massive cleanup or even a complete rewrite.
I think the best solution here is to try to create a new project in a clean workspace, and using the wizard.
Thanks for the suggestions.