lpcware

LPCXpresso 4.0.5 - cr_startup_lpc13.c import problem

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by pwiszowaty on Sun Jul 31 12:23:49 MST 2011
There is a problem when creating a new project in LPCXpresso 4.0.5 on Fedora 15 64-bit: IDE throws a NullPointerException after clicking "Finish" and the created project is missing src/cr_startup_lpc13.c. The src directory contains only main.c file. The project can be compiled but can't - obviously - be run on a microcontroller.
The workaround (pretty inconvinient) is to import the missing startup file from any of the example projects.
Attached exception stacktrace from .metadata/.log.

What might be the cause of the import failure ?

Outcomes