Content originally posted in LPCWare by frame on Mon Aug 27 01:04:46 MST 2012
Quote:
[SIZE=4]What happens if the input voltage is not held steady and varies[/SIZE]
[SIZE=4]significantly during the conversion?[/SIZE]
[SIZE=4]
[/SIZE]Short answer: this is your problem
Longer answer: this is primarily not of concern. During the (actual) conversation, the S/H is
in the [B]Hold[/B] phase, it ignores all changes on the input at that time. That's the very purpose of it.
Of much greater interest are the changes of the input signal during the [B]Sample[/B] phase.
The sampling element is basically a capacitor, which is charged by the input signal over
the source impedance and the input resistance. The voltage that capacitor is charged to is a
measure of the average (in a broad sense) of the input voltage during the sampling time.
So it's your turn to take care about signal variation. A low pass filter might be a good idea in most cases.