Content originally posted in LPCWare by jdeas on Tue Jul 22 15:37:39 MST 2014
Interesting. I don't have the CANopen ROM API, just the provided CCAN_API header file and example.
If the ROM is using 'random' memory blocks then I'm surprised I got this far. I would assume that I need to both reserve AND reference the location for the ROM driver.
Considering the LPCXpresso example does not show the need for RAM outside msgblks and the subcall return block, where can I get the actual API showing a proper CCAN init?