lpcware

Feature Request - MCU Settings Dialog according to build configuration

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by acelery on Wed Aug 29 07:44:33 MST 2012
Hi, I wrote a few static libraries to abstract my applications from the underlying hardware, so if I want to build againts an LPC1343 I just -lLPC1343, and if I want to build againts an LPC1769 I just -lLPC1769. I have created two build configurations that target the different libraries, but after I change the build config I have to also change the target MCU in the "MCU Settings Dialog" (which does not support settings according to build configurations).

Could this feature please be added to a future release of LPCXpresso? I figure it's not to difficult to do.

Thanks a lot!

Regards,
Alex

Outcomes