Content originally posted in LPCWare by robert.palmer on Mon Aug 27 09:32:31 MST 2012
As far as I know, I never turned on CRP. I shouldn't have a hardware problem - as you can see, I've tested the board using the scope with resets and interrupts, I've been able to determine that it is actually running and that it is responding to the wake-up interrupt correctly. The problem seems to be that the RedProbe+/debugger can't catch it before it goes to sleep.
Again though, if I press the Debug option from Eclipse, and watch the reset line going to the chip, (I have the scope set to capture a single event), I NEVER see the debugger cause the reset line to activate. I get the connection error, but never a reset. I would have thought the first thing it would do would be try to reset the chip, then attempt to connect, then do whatever else (program the chip, erase, etc).
I will try a couple more attempts - mass erase and FlashMagic to see if I can gain access.