lpcware

LPCXpresso example project for Hitex LPC1857 Eval Board

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by eX-SNB on Tue Nov 05 07:34:24 MST 2013
Hello,
I'm a beginner with the LPC1857.

I have the Hitex LPC1857 Eval Board.
I try to use a example project from LPCopen for testing the board, but the examples are only for the LPC1850.
If I compile the example code the axf file is generated, but debugging from the board is not possible.
My example program is the "lpc18xx_hitex_eva_1850_periph_blinky".
This example use the external SPIFl.
The Boot-Pins from the board are configured for SPIFl
Boot1 --> 1-2
Boot2 --> 3-4
Boot3 --> 3-4
Boot4 --> 3-4

Have anyone an idea what I can do to run the example on the LPC1857 Hitex Eval Board?
Otherwise if anyone have an example for the Hitex LPC1857 that were very helpful for me.
Thanks

Stefan

Outcomes