Content originally posted in LPCWare by paul.rcom-software.com on Thu Jul 24 14:30:33 MST 2014
I am using an Embedded Artists LPC4088-32 dev. board with the Rowley Crossworks toolchain and
LPCXpresso. Does anybody know if the EMWIN graphics package has been successfully ported
to this environment--or a close one ?
This is the information about the graphics hardware I plan to use.
* On-Board LCD Controller
LCD controller, supporting both Super-Twisted Nematic (STN) and Thin-Film
Transistor (TFT) displays.
- Dedicated DMA controller.
- Selectable display resolution (up to 1024 × 768 pixels)
Selectable display resolution (up to 1024 × 768 pixels)
Features and capabilities are detailed in chapter 11 of the NXP UM10562 LPC407X/408X User Manual.
NOTES: To be used in conjuction with a Kyocera 3 1/2" QVGA LCD display--model
number T-55343GD035JU-LW-ADN
Best Regards,
Paul R.