Content originally posted in LPCWare by paul.rcom-software.com on Fri Jul 25 15:22:19 MST 2014
Does NXP provide the following compoents for the integral LPC4088 MCU USB hardware per chapter 12 and 13 of
the NXP UM10562 LCP408x/407x User Manual ?
* Driver
* USB Device Stack with the CDC/ACM class.
* A convenient API for data transfer.
The following link seems to describe something which has those components.
docs.lpcware.com/usbromlib/v1.0
Can this library be used in conjunction with or under FreeRTOS or a similar RTOS ?