Content originally posted in LPCWare by wdawson61 on Tue May 03 15:31:21 MST 2011
[B]Lpcxpresso Linux 3.83
Linux 10.04
LPC1754 project
[/B]
I have a project that has a main folder with source files as well subfolders that contain more source files. If I place a syntactically-correct call to a non-existentfunction in one of the source files contained in a sub-folder, the executable is built with only a minor gripe about "implicit declaration." If I place a syntax error in the module, the compiler sees it and no executable is built.
If, however, I place the same bogus function call (to a nonexistent function) in one of the source files of the main project folder, I get thet expected "reference to undefined function."
wtf??
Regards,
Wade