Lpc1114/302

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc1114/302

240 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zved17 on Sat Apr 23 14:20:03 MST 2011
Hi,

I am trying to use the  LPC EXpresso 1114/302 board, using

[SIZE=1][LEFT][SIZE=4]LPCXpresso: [/SIZE][/LEFT]
[SIZE=4]Build id: LPCXpresso v3.4.0 [Build 187] [23/06/2010] ;[/SIZE]
[SIZE=4][/SIZE]
[SIZE=4]This build do not have the option of selecting PC1114/302 in[/SIZE]
[SIZE=4][/SIZE]
[SIZE=4]Project  --> Properties  --> C/C++ Build --> MCU Settings[/SIZE]
[SIZE=4]                                                           -->lpc1100[/SIZE]
[SIZE=4]                                                           --> ...... [/SIZE]
[SIZE=4]Pl, help.[/SIZE]
[SIZE=4][/SIZE]
[SIZE=4]Thanks.[/SIZE]
[/SIZE]
0 Kudos
1 Reply

222 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Apr 23 14:23:20 MST 2011
Use:

http://lpcxpresso.code-red-tech.com/LPCXpresso/

to download a new version of LPCXpresso :)
0 Kudos