lpcware

hex file does not run when download with Flash Magic

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Dan Griffin on Thu Apr 17 05:45:34 MST 2014
Have created a simple "blinky" project which runs just fine with the LPCxpresso download to a target LPC1114/301 processor on the OM11049 board. I use the format
arm-none-eabi-size ${BuildArtifactFileName}; arm-none-eabi-objcopy -O ihex ${BuildArtifactFileName} ${BuildArtifactFileBaseName}.hex ; to create the hex file. which all works just fine. The hex file is then downloaded to a custom board using Flash Magic. Flash Magic reads the target "LPC11114/302 device code back correctly and the code is download and verified correctly, however, the code just fails to run. Any suggestions to get the simple code to work! Have tried on two different boards, so don't think their is a problem with the custom target!

Original Attachment has been moved to: BLINKY.zip

Outcomes