lpcware

Wrong Known LPC1758 ID(s): 0x25013737

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by thomas on Mon Jul 05 07:15:27 MST 2010
Trying to download to a LPC1758 on Keil eval board, MCB1700, using
LPCXpresso ver. 3.4 and LPC-link.
Got the following error:
LPCXpresso Debug Driver v2.0 (Jun 10 2010 11:46:27)
Looked for chip XML file in C:/nxp/lpcxpresso_3.4/bin/LPC1758.xml
Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.4/bin/nxp_directory.xml
Found generic directory XML file in C:/nxp/lpcxpresso_3.4/bin/crt_directory.xml
Invalid LPC1758 Part ID: 0x25013F37
Known LPC1758 ID(s): 0x25013737
03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part

Reverted to LPCXpresso ver. 3.3.4 - works fine.

Flash Magic uses Signature: 0x25013F37, for the LPC1758, so
it seems to me that there is an error in LPCXpresso ver. 3.4.

BR/Thomas

Original Attachment has been moved to: 1100516_npe.txt.zip

Outcomes