All:
Some great discussion on BDM.
Couple of interesting bits...
A new "open-source" updated design is coming soon. Finishing firmware, will use hardware with slightly more memory and will allow the same basic hardware design to be used for S08, V1 ColdFire, and V2-V4 ColdFire.
As for the P&E BDM. I believe CodeSourcery does have a GDB stub driver for the P&E USB wiggler.
Probably need to draw more attention to that..
Also, the 5445x board does have the P&E wiggler built into the board. As do a lot of our newer EVBs. And the 5445x board does have Uboot, so you can reflash the second flash with your test kernel, firmware, etc... and then flip switch 1 on the board and the board will boot from the other flash. This allows you to keep your protected Uboot on the small boot flash, and then use the other flash for development. Technically, you don't need a wiggler or probe at all, if you just use Uboot to download and PrintF, Printk, etc... for debug messages.
Hope this helps...
I'll post when the new open source design becomes available.
-JWW