lpcware

problem compiling "c++" file with LPCXpresso

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by aferrari on Tue Sep 01 05:28:07 MST 2015
Hello everybody,

I'm using LPCXpresso v7.9.0 on Windows8 Pro.

I've done a C project with included some c++ files.

I'm able to complile *.c files (for example foo_1.c), but I'm not able to compile c++ files.

For example if I try to compile foo_2.cpp in the following way:

1) right click on this file in the "Project Explorer" tree
2) select "Build Selected File(s)"

the LPCXpresso doesn't run the compiler like does with the foo_1.c file.

I mean that in the "Console" window the compiler is not launched.

Any idea about this issue?

Thanks in advance

Alberto

Outcomes