Content originally posted in LPCWare by richas on Thu Feb 07 11:47:48 MST 2013 I have the need to read out the code from a LPC1114/301. The device is not protected. I see the LPCxpresso IDE and command line tools for programming but nothing for reading a device.
Is there a tool for reading a devices flash into a .axf or .bin file?
Content originally posted in LPCWare by richas on Thu Feb 07 16:59:15 MST 2013 I am opening the debug perspective, and the a memory browser. I find a point past the end of the code and export to a bin file.
Content originally posted in LPCWare by wrighflyer on Thu Feb 07 15:22:12 MST 2013 When I first got the LPC812 Xpresso I wanted to read the code out. When I googled I hit an article on the Code Red site. It said to edit a debug profile and just change the option so it doesn't start by downloading code. When you start debugging you can then select the function to read back flash.
Content originally posted in LPCWare by MikeSimmonds on Thu Feb 07 12:52:34 MST 2013 [FONT=Trebuchet MS][SIZE=1]My usual plan is to debug the device (make sure you set load to false) then hit suspend. I then open a memory view to cover the flash and use the export button.
I understand that FlashMagic has commands to read from the device. I have never used it and don't know what (if any) export options it has.