lpcware

CRP on LPC4330 and external flash

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by tgiacomelli on Wed Jan 30 12:04:06 MST 2013
Hello,

  It's really difficult to have information about CRP configuration on LPC4330 with external SPI Flash. So I can't even be sure than this is supported. If anybody can point me to the right information, I would appreciate.

  Anyway I've tested it, but build failed:[SIZE=3] [B]Linker CRP Enabled, but no CRP_WORD provided within application[/B]

  The CRP_WORD is configured properly, so there is no[SIZE=3] reason to that message.

[SIZE=3]  We have also tried to force the CRP in the ld file but it [SIZE=3]has no effect[SIZE=3]. The point is that we don't know where to set the CRP value in the external flash or in[SIZE=3]ternal RAM this is not specified in the documentation.
[/SIZE][/SIZE][/SIZE][/SIZE][/SIZE][/SIZE]

Outcomes