Content originally posted in LPCWare by kuldip rajput on Tue Mar 03 02:16:59 MST 2015
Respected Sir,
I have attached the sample code of the framework that i am following. The code is not showing any error, but i am unable to show the result in the console view of Lpcxpresso IDE. I have did the setting change in the quick panel menu-> edit project settings->settings->MCU Linker->settings-> redlib(semihost). But still i am unable to print any statement from the main.c and other files to. Please suggest me the possible solution regarding this problem.
I am getting following errors-
Description Resource Path Location Type
1)make: *** [FreeRTOS-Plus-Demo-1.axf] Error 1 C/C++ Problem
Description Resource Path Location Type
2)make: *** [Source/debug_frmwrk.o] Error 1 C/C++ Problem
Description Resource Path Location Type
3)make: *** [Source/FreeRTOS-Products/FreeRTOS-Plus-IO/Device/LPC17xx/FreeRTOS_lpc17xx_can.o] Error 1 C/C++ Problem
Description Resource Path Location Type
4)make: *** [Source/lpc17xx_adc.o] Error 1 C/C++ Problem