Is there a sample for DFU with usbd_lib?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a sample for DFU with usbd_lib?

346 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sposnjak on Tue May 27 01:24:41 MST 2014
Hi all!

Is there a sample for DFU with usbd_lib? I can only find HID, MSC, CDC samples. If anyone can provide one for DFU I would be very grateful.

Thank you.

Labels (1)
0 Kudos
1 Reply

319 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Fri May 30 13:35:57 MST 2014
There is a DFU example for ROM based USB drivers in the v2.12 package for LPC4370. The USB ROM drivers API is the same for all parts that have USB ROM drivers so this should work for whatever chip you are using.
0 Kudos