#define LPC_CAN0_BASE 0x40050000 |
/*------------- CAN Controller (CAN) ----------------------------*/ /** @addtogroup LPC11xx_CAN LPC11xx Controller Area Network(CAN) @{ */ typedef struct { __IO uint32_t CNTL;/* 0x000 */ __IO uint32_t STAT; __IO uint32_t EC; __IO uint32_t BT; __IO uint32_t INT; __IO uint32_t TEST; __IO uint32_t BRPE; uint32_t RESERVED0; __IO uint32_t IF1_CMDREQ;/* 0x020 */ __IO uint32_t IF1_CMDMSK; __IO uint32_t IF1_MSK1; __IO uint32_t IF1_MSK2; __IO uint32_t IF1_ARB1; __IO uint32_t IF1_ARB2; __IO uint32_t IF1_MCTRL; __IO uint32_t IF1_DA1; __IO uint32_t IF1_DA2; __IO uint32_t IF1_DB1; __IO uint32_t IF1_DB2; uint32_t RESERVED1[13]; __IO uint32_t IF2_CMDREQ;/* 0x080 */ __IO uint32_t IF2_CMDMSK; __IO uint32_t IF2_MSK1; __IO uint32_t IF2_MSK2; __IO uint32_t IF2_ARB1; __IO uint32_t IF2_ARB2; __IO uint32_t IF2_MCTRL; __IO uint32_t IF2_DA1; __IO uint32_t IF2_DA2; __IO uint32_t IF2_DB1; __IO uint32_t IF2_DB2; uint32_t RESERVED2[21]; __I uint32_t TXREQ1;/* 0x100 */ __I uint32_t TXREQ2; uint32_t RESERVED3[6]; __I uint32_t ND1;/* 0x120 */ __I uint32_t ND2; uint32_t RESERVED4[6]; __I uint32_t IR1;/* 0x140 */ __I uint32_t IR2; uint32_t RESERVED5[6]; __I uint32_t MSGV1;/* 0x160 */ __I uint32_t MSGV2; uint32_t RESERVED6[6]; __IO uint32_t CLKDIV;/* 0x180 */ } LPC_CAN0_TypeDef; /*@}*/ /* end of group LPC11xx_CAN */ #define LPC_CAN0 ((LPC_CAN0_TypeDef *) LPC_CAN0_BASE) |