MC13213 RF Characterization Testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213 RF Characterization Testing

941 Views
GaryOlmstead
Senior Contributor I
Hi --
 
We are rolling our own ZigBee board with an MC13213.  For the required RF testing, we would like to be able to transmit continuously.  I don't see any way to do that.  Is there some undocumented test mode that would allow us to do this?
 
Gary Olmstead
Toucan Technology
Ventura CA
 
Labels (1)
0 Kudos
1 Reply

169 Views
Mads
Contributor V
Hi Gary,
 
My suggestion would be to used one of the documented ways :smileyhappy:
 
If you are using the SMAC you can use the Test mode application which contains all kinds of test features including continous TX.
 
if you are using Beestack or MACPHY you can use the "telec" test commands which are described in the MACPHY reference manual. these allows you to do Cont. Rx and TX.
 
Br,
Mads
0 Kudos