Content originally posted in LPCWare by RatheeshT on Tue Jan 12 06:09:27 MST 2016
Hi ,
When i am running or debugging my application in LPCXPRESSO , program control comes into the below function
__attribute__ ((section(".after_vectors")))
void SysTick_Handler(void)
{
while(1)
{
}
}
( which is available in the " cr_startup_lpc11axx.c ")
Queries are :
1. Whether is this behavior normal or not ?
2. can i add my part of codes here?
3. if it is not correct , please give me your suggestions
Hardware: LPC11Axx series
Platform : Windows-7
IDE : LPC Xpresso 7.9
Thanks in advance
Regards,
Ratheesh T