lpcware

SD CARD DRIVER ERROR

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Gonzalo_Sipel on Thu Nov 20 12:34:45 MST 2014
Hello:
         I'm working with a LPC1788 and I'm using the SD interface.
My problems is in [color=#c33]Chip_SDMMC_WriteBlocks()[/color] function which is into the[color=#c36] sdmmc_17xx_40xx.c[/color] file. This problems occurs when I try to write more than 512 bytes in the same write operation because the function gets stuck waiting the transfer state:

[color=#c30]while (Chip_SDMMC_GetCardState(pSDC, pCardInfo) != SDMMC_TRAN_ST) {}[/color]

Has anyone had a problem like this?

Outcomes