Content originally posted in LPCWare by TravisT on Tue Dec 10 14:19:42 MST 2013
I have figured out at least the base of my issue. I was using one of the open drain pins which does not seem to work, at least without more configuration. I jumper-ed to another free pin and used the switch matrix with successful results.
I have not fully tested the SPI communication yet, but with what I have now I should be able to move forward.
In regards to the open drain pin, will it not work as a UART pin? Do I need to do some extra configuration with the pin mode in order to utilize it? I was under the assumption it was more configurable.
Thanks