Content originally posted in LPCWare by HammingBird on Sun May 29 08:25:39 MST 2016
Hallo,
I am using "LPC810".
I would like to ask about LPC810 "Deep Power Down" mode. see more in user Manual --> 5.7.7
_______________________________________________________________________
5.7.7 Deep power-down mode:
During Deep power-down mode, the contents of the SRAM and registers are not retained
except for a small amount of data which can be stored in the general purpose registers of
the PMU block.
____________________________________________________________________
As I understood, in Deep power-down mode, once LPC810 enter in "Deep power-down mode" prog memory prog will be erased.
is it right ?
if so, then how LPC810 will work after wake up ? coz, prog has been erased ?
Thanks