Content originally posted in LPCWare by Pat on Mon Nov 23 04:07:48 MST 2015
Hi A,
Indeed nothing wrong here, the remark is only made to make people aware that in default pin configuration the silk screen print can cause confusion: The LPC pin routing to J6 pin 40 and 41 ( PIO0_10 and PIO0_11) is correct, but the silk screen label gives the impression that PIO_010 is SDA and PIO0_11 is SCL. But that is the other way around in default configuration for an LPC81x !
Thanks for pointing out the possibilities to use the switch matrix to swap to pin function for these two open-drain pins.