Content originally posted in LPCWare by starblue on Wed Apr 29 00:24:49 MST 2015
Quote: trimarco232
well, I assume that the 4 compare match registers you refer to are the 3 pwm duty cycles and the 4th for the max of the the PWM?
Yes.
Quote:
Is there a way to avoid the 4th ?
I don't think so, unless maybe when your period is exactly 2^16 clock cycles, which is not the case.
Quote:
Quote:
the LPC82x, it has a bigger SCT
price is not an issue, but the 16TSSOP size is the best for my project, because I have no more room on my PCB, and my skills don't allow me to solder TQFP packages
It is available as TSSOP20 and HVQFN33, not TQFP. HVQFN33 is about the same size as TSSOP16, but I would also consider it difficult to solder (I haven't tried QFN yet, TQFP is fine with me).
TSSOP20 is just 1.3mm longer than TSSOP16, is it really that tight on your board?