Content originally posted in LPCWare by remcopoelstra on Sun Aug 31 07:16:13 MST 2014
Hi,
I've based my code on the UART ringbuffer example to send and receive bytes (almost an exact copy).
I'm missing lots of bytes though.
Sometimes a few get through, sometimes even about 100. But in the end I always miss bytes.
The Ringbuffer_GetCount simple tells me it's empty.
How reliable is the ringbuffer+uart combination?
Can the ringbuffer handle being fed by the interrupt handler while also being interrogated from the main loop?
Regards,
Remco Poelstra