USB-HID communication with 13213-NCB(Network Coordinator Board)
Hi,
I am using the 13213-NCB which uses the 8bit MC13213 mcu. I have the following questions:
1) Can this device be used as a USB-HID client for doing HID communication with a host PC?
2) The board has a SILABS CP2102 mcu next to the usb port. Is this the mcu that is used for USB connectivity?
3) Which mcu on the board should be used for doing USB-HID programming and communication?
Regards,
-EB
Message Edited by Embedded Boy on 2008-05-16 11:36 AMMessage Edited by Embedded Boy on 2008-05-16 11:37 AM