LPC5411x MCU family announced

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5411x MCU family announced

279 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 01:45:04 MST 2016
NXP Semiconductors N.V. (NASDAQ: NXPI) today introduced its next-generation family of low-power, multi-market MCUs – the LPC5411x. With today’s introduction, NXP extends its LPC54000 series of MCUs with improved power efficiency, a host of serial peripherals, flexible run-modes, autonomous operations when the CPU is not active and voice-detection DSP hardware.

The LPC5411x are ARM Cortex-M4 based microcontrollers for embedded applications.These devices include an ARM Cortex-M0+ coprocessor, up to 192 KB of on-chip SRAM, up to 256 KB on-chip flash, full-speed USB device interface with Crystal-less operation, a DMIC subsystem with PDM microphone interface and I²S, five general-purpose timers, one SCTimer/PWM, one RTC/alarm timer, one 24-bit Multi-Rate Timer (MRT), a Windowed Watchdog Timer (WWDT), eight flexible serial communication peripherals (each of which can be a USART, SPI, or I²C interface), and one 12-bit 5.0 Msamples/sec ADC, and a temperature sensor

For more information see:
[list]
  [*]LPC5411x Press release
  [*]LPC5411x Product page
[/list]

Labels (1)
0 Kudos
0 Replies