Content originally posted in LPCWare by louislo on Sun Mar 30 19:51:21 MST 2014
Okay, so i managed to run it in ISP mode by pulling pin 2.10 to ground, and then able to program it using Xpresso when the issue mention above occurs. Only that it didn't solve the issue since it still encountered error after a power reset.
The board i using is prototype design, not commercially available.
So here is what i do,
1. I used keil's Uvision and opened up the software's sample project for MCB2300 which uses the same chip, project named RTX_blinky and downloaded the flash code into the board. The board blink's it's led which confirm the code is working.
2. I used LPCXpresso and used the new project wizard to create a new blank program for LPC2388, without any additional source code. I mass erased and power reset, no probs there as the board and jtag device can still be detected.
3. I programmed the blank program in, flash done, power reset and error occured.
4. Reset the board to run on isp mode, programmed the axf genereated by keil RTX_blinky sample project, and the board went well even after power reset.
Xpresso i am using is LPCXpresso v7.0.0
i am aware there is slightly newer version, but i had tested it out at diff computer, still the same.
Regards,
Louis